This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54560: TPS54560

Part Number: TPS54560

Hi TI team,

We have designed power supply circuit using TPS54560DDAR IC, today we were doing board check.

As per the circuit, VIN is the Input 48V from the Battery and when the Keyswitch is a ON/OFF, If the Switch is closed, VCC_48V is geneated and the same voltage is connected to TPS54560 IC.

I started the board check up by giveing VCC_IN(48V) and afer 30 sec I made the keyswitch ON, I got the sound from relay, then 5V was coming,

After that, I made the Key switch OFF, Till here no issue, Then when I again made the Keyswitch ON, I THe TPS54560 IC blown off at its input side.

I couldn't get any reason for this cause, Kindly support on to this resolve.

Thanks

TPS54560DDAR_TI_review.pdf