Hello,
I have a customer planning to use the TLV70730 in an application. However, there are times when his battery may dip below 3.0V say down to 2.8V. He sees the output voltage follow the input voltage down with a slight drop. Is it reasonable to say that in the condition of VIN<3.0V in the case of the TLV70730 that the TLV70730 will regulate to the input voltage minus the drop out voltage and this will work down to an input voltage of 2.0V? Do we have any graphs or data for this condition?
Thanks for your feedback.
-Will Jarrett