Other Parts Discussed in Thread: PMP9616, PMP, CSD17570Q5B
Hi
Customer have a question about PMP9616 data.
In "Start up waveform", 1.5 A flows for 40 ms.
(As PMP 9616 FETs are used in parallel in , the current flowing through one FET is considered to be about 0.75 A.)
The customer has almost the same specification as PMP 9616, but since the ambient temperature is max 75 ° C, I am concerned whether there is a problem at startup even at that temperature.
Best Regard
T Kishi