TI`s engineer:
How do you do?
I have some questions about TPS65262. The following question is it.
Number one: if MODE pin connect to GND, it will mean the enable function will depend on external device, such as MCU.Must be set as open drain output, it need have in series with resistor. Whether the resistor is needed? such as: MCU ---> resistor ---> EN pin.
Number two: if MODE pin connect to GND, it will mean the enable function will depend on external device. i use two resistors divide by Vin(12V), whether the resistance in accordance with following formule. Or select two resistors(the resistance don`t care) to get the voltage rather than threshold of EN pin.
Number three: if MODE pin connect to GND, and use two resistor to get voltage rather than threshold of EN pin. And the UVLO how to set if base on the following formule ? The Vstart and Vstop means...?
Thank you very much!
The following content form page 15 of TPS65262`s datasheet.