This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5000: Isolated Configuration with Opt-Isolator?

Part Number: LM5000
Other Parts Discussed in Thread: LM5015, , LM5001

Hello All,

My customer is using the LM5000 in non-isolated flyback configuration, it would be possible to use in isolated configuration with opto-isolator feedback (for example, as the LM5015 which is done for forward), is there a reference design for that?


If it were not possible, would you be able to show me a component with an integrated switch of at least 75V where the above can be done?

Many Thanks,

Antonio