Other Parts Discussed in Thread: LM2990, LM79, LM337-N
Hi all,
Can LM2940C be used for Negative voltage?
Because LM2990 is too much High-cost. My customer rejected it.
If you have the idea for negative voltage use, please teach me the circuit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The LM2940C was designed as a positive LDO voltage regulator with a recommended operating input voltage of 6 V to 26 V. To ensure consistent and reliable operation, this device should not be used with a negative input voltage.
The LM337-N and the LM79 are some examples of TI's negative voltage regulators that are cheaper than the LM2990 and support at least 1 A load current. If you provide more information about your customer's application I will be able to make a more specific recommendation. You can also parametric search TI's LDO and linear regulator portfolio based on your customer's requirements here:
http://www.ti.com/power-management/linear-regulators-ldo/products.html
Thanks,
Gerard
Hi,
Thank you.
But they need "LDO".
Your suggestion is not LDO.
They accepted LM2940C price.
So I need the reason why same internal component LM2990 is much higher price.
Can you assert that the LM2940C sells 100 times more quantity than LM2990?
If so, I can explain it to the customer.