Dear all.
Please teach me about reverse current.
Reverse currrent is written in the data sheet as follows.
--------------
The NMOS pass element, by design, contains no body diode.
This means that, as long as the gate of the pass element is not driven, there is no reverse current flow through the pass element during a reverse voltage event.
The gate of the pass element is not driven when VBIAS is below the UVLO threshold, or when the EN pin is held low.
--------------
When EN is High and UVLO exceed the threshold, does a reverse current flow?
Is the MOSFET back to back coupling?
Regards,
PAN-M