Hi team,
My customer wants to use the TPS3700 in their system. i have some questions want to check with you.
1. The supply and monitor voltage are the same(12V). if the voltage has variation during operation, whether the devices has problems? From the datasheet, it seems to be fine.
2.The UV is 10.8V, OV is 13.2V.
The internal reference voltage is only 0.4V. My customer has concern about so low reference voltage, whether it has risks? for the divider resistor value, do you have some suggestions? Do we have some higher reference devices?
whether the excel result is ok?
Feel free to let me know when you have other recommendations.
Thanks.