Hi all,
Battery is LiPo 90mAh.
Charging current (IOUT)is 20mA. ->K = 320, -> RSET = 39K.
with the above parameter, ITERM is 2mA, which is below the minimum ITERM 5mA (datasheet).
Is it possible for the controller to detect Charge Done condition if the ITERM is less than the minimum?