Other Parts Discussed in Thread: LM36010, LM3644
Dear TI Experts,
My customer has below requirment for LED driver:
1) Input Voltage 3.3V (or Li-battery directly power from 3.7~4.2V)
2) 2 channel total, 1 channel is capable of providing 1.6A peak current for laser LED (3.4~3.6V), driver will work with less than 1 sencond every time, most time it is in sleep mode to save power;
another channel is similiar function only with less peak current around 1.3A
For this application, it seems to need 2pcs TPS61310 to drive 2 LEDs seperated.
Could you kindly help to give some advice about such requirment? Is there any single chip solution or better 2 chips solution?
Thanks a lot.