This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reset time of TL7700

Other Parts Discussed in Thread: TL7700

We have a question about TL7700.

Question 1.

Please tell us the reset time(min / typ / max) of TL7700.

We understand that reset time is the time from detecting overcurrent to reset signal output.

We want to know the variation of reset time.

We hope for an earlier response.

Best regards,

Takahiro Nishizawa

  • Takahiro,

    For this device, we only provide the typical delay. Things like operating conditions and capacitor tolerance will have slight impact on delay accuracy.

    Typical delay is given in section 8.3.3 Output Pulse-Duration Setting of the datasheet.

    tpo = Ct × 10^5 seconds
    where Ct is the timing capacitor in farads.

    Please refer to Figure 6 and let me know if you have additional questions. Thank you!

    -Michael
  • Thank you for your answer!

    We understand that reset time is calculated by the following formula.
    tpo = Ct × 10^5 seconds

    We think this formula is typical value.
    Do you have the data about the variation?
    For example, ±%
    Is it difficult to check the variation of reset time?


    Best regards,


    Takahiro Nishizawa
  • Takahiro,

    Unfortunately since this device was created in 1999, not much data exists on this device. We have newer Wide Vin devices that have been better characterized. For TL7700, all we have are the typical curves to suggest an approximate delay. Factors such as operating temperature, capacitor tolerance, parasitic capacitance on the reset pins will degrade delay accuracy. From the Output Pulse Duration spec in table 6.6 which specs the delay with CT = 0.01uF, we see that the accuracy can vary up to +/- 50% absolute worst case. We often times see the delay accuracy to be better than +/- 50% but it is not something we have enough data to make a guarantee. The best thing to do is test the device in your specific application to see if the performance will meet your needs. Also, use accurate capacitors to minimize error.

    Please let me know if you need additional support with this. Thanks!

    -Michael
  • Thank you for your answer!

    Variation of reset time is +/- 50% absolute worst case.
    Is this understanding correct?

    Best regards,

    Takahiro Nishizawa
  • Takahiro,

    Yes that is correct.

    -Michael
  • Thank you for your answer!


    We have new questions.
    We don't use the external capacitor of CT pin.

    Question.1
    Is the reset time 10µS(typ) when we don't use the external capacitor of CT pin?

    Question 2.
    Reset time is 15µS(max) and 5µS(min) when reset time(typ) is 10µS.
    Because variation of reset time is about ±50%.
    Is this correct?

    Question 3.
    Please tell us the terminal processing of CT pin when we don't use the external capacitor of CT pin.
    Open? connect to the GND?


    Best regards,


    Takahiro Nishizawa
  • Thank you for your answer!


    How is your situation?
    We hope earlier answer!


    Best regards,


    Takahiro Nishizawa
  • Thank you for your support!

    In datasheet p.3 CT pin,
    even if CT is set to 0, response speeds remain at approximately 5 to 10 µs.

    And you said "we see that the accuracy can vary up to +/- 50% absolute worst case."


    When Ct=0

    min=5µS
    typ=10µS
    max=15µS

    Is this correct?

    And please tell us the terminal processing of to set forrlowing conditon.
    even if CT is set to 0, response speeds remain at approximately 5 to 10 µs.

    Open or Connected to GND and so on.

    We hope earlier answer!


    Best regards,


    Takahiro Nishizawa
  • Takahiro,

    Answer 1. If no capacitor, the device response speed is approximately 5us to 10 us according to section 8.3.3 in the datasheet. The capacitance on the output will also impact the response time.

    Answer 2. This is correct for absolute worst case under all operating conditions. Under normal operating conditions, the delay will be closer to the typical value.

    Answer 3. Leave CT pin floating if not using a capacitor.

    Please let me know if you have additional questions. Thanks!

    -Michael
  • Takahiro,

    You are correct in your assumption. Please leave CT pin floating if not using a capacitor. Thanks!

    -Michael