This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD95480RWJ: can CSD95480 meet +/- 4% current sense accuracy at below condition range?

Part Number: CSD95480RWJ

Hi 

customer want to check if CSD95480 can meet +/- 4% current sense accuracy at below condition range?

: Vin=7V to 13.2V range, Vo=0.6V~3.3v range,Vdrvi=5V,  Tj=25C~125C ,25A<Iout<45A 

if CSD95480 can't meet +/- 4% current sense accuracy,

is there any other device can meet this requirement and it is p2p with CSD95480 ?

thanks.