This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM84A22: Could you please help check with power loss analysis to see how many load is ok (not trigger over temperature)for the module based on the customer's set up?

Part Number: TPSM84A22

Hi team,

My customer tested our EVM board with VIN 12V, Vout 1.8v, load 10A, no fan, ambient 95°C, and find the device will trigger thermal shutdown.

You know the module's performance will change based on the device variation. So they cannot get the result based on one board test result.

Could you please help check with power loss analysis to see how many load is ok (not trigger over temperature)for the module based on the customer's set up?

Thanks.