This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61236EVM-676: TPS61236EVM-676

Part Number: TPS61236EVM-676
Other Parts Discussed in Thread: TPS61236P, TPS61230A

HI,

I would contact my TI FAE, but he is out this week. I am interested in using this EVM for a design that is using the TPS61236PRWLR, but I see that the EVM has a TPS6123RWLR chip on it.  Is this chip the same as the P chip? Why is this EVM recommended for the TPS61236PRWLR? 

Also the inductor on the EVM is a 21A Coilcraft XAL7030-102MEB 1UH 64mm2.

My design will only need to draw 1.5A, and as such Webbench selected a 1.0UH Murata DFE252012F (10 mm2)  3.8A. 

Thank you very much for your help.

Jeff Cohen

Dentsply Sirona Inc. Long Island City, NY 11101