This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2511-Q1: How to design TPS2511 of hardware

Part Number: TPS2511-Q1
Other Parts Discussed in Thread: TPS2511

Dear TI,

I am examining TPS2511-Q1 for USB charger of vehicle.

I have some questions.

1. When I checked EVM, Rilim is applied 1/10W(1608 size).

    Should I apply 1608 size for Rilim?

2. When I checked document of SLVA800(Effective system ESD protection guidelines), Ferrite Bead was applied(figure 4) 2012 size for D+ and D-.

    Why there are applying 2012 size?

3. I checked protocol of TPS2511.

    What is mean Divider mode?

4. When I short test of USB lines(VBUS, D+, D-, GND), is there some document about test result?

   Short test condition as below.

  -> +12V to VBUS,   

  -> +12V to D+,   

  -> +12V to D-,   

  -> +12V to GND

Please help for these.

Thanks.

  • Hi, Jeongtae Park,

    1. You can apply 1608 size or any other size, it doesn't matter.
    2. It depends on your layout. The size don't have much influence.
    3. Divider mode means special DCP mode for Apple device and Samsung. As you know, DCP mode defined by USB-IF just allow 1.5A max charging current. Samsung and Apple defined their own DCP mode for max 2.4A charging current, we call it DCP divider mode.
    4. The Abs max voltage on those pin of TPS2511 is 7V, so 12V will damaged TPS2511. I suggest you to add TVS diode for this case.

    Regards,
    Bob