Other Parts Discussed in Thread: TL1963A
Dears,
I use TL1963A-Q1 to convert 13.5V input voltage to 12V output voltage, with the ShutDown pin of TL1963A-Q1 being controlled by external controller. Please see the schematics below.
When the ShutDown pin is pulled low and the IN pin is 13.5V, I get 1.59V at the OUT pin which is expected to be zero or a very low voltage. Could you please explain why there is a relatively high voltage at the OUT pin while I pulled down the ShutDown pin?
When I put a parallel resistor of 1k ohms to the OUTpin, I get a voltage of about 0.2V. So I think it might be the leakage current that makes the non-zero output voltage. But it does not make sense since the leakage current is only several amperes when in shutdown mode by the datasheet.
Thank you very much.
Regards,
Tang Yaosheng