Part Number: TPS23753AEVM-004
Hi,
Reading the users guide for the TPS23753AEVM-004 board, I am looking at validating the operation at 5V under 10W load, with a 12V AUX input.
First, I will change the components listed in the BOM for 5V output operation (for example T2 use a HA3802-BL)
Can I substitute Q2, Si4848DY for a Si4848ADY? I assume the A suffix denotes an improved part (higher current operation).
Can I also lower R18 from 390 mOhms to say 220mOhms to achieve extra current at 12V input (knowing that the flyback transformer can handle it)?
Thanks in advance,
Kyran McGlasson
SAGE Automation - Australia