This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5118: it is possible to take 7 to 35v input and 48 v 5A output using this IC

Part Number: LM5118
Other Parts Discussed in Thread: LM5122

i need the application take the input 7 to 35 v and 48v 5A output. it is possible ?

I cant able to simulate using webench for this Propose.

  • Hi Vignesh,

    Thank you for reaching out with your question.

    It is possible to use the LM5118 for this design but is probably not the best choice. I suggest using the LM5122 for this design. Based on the application specification you provided a boost controller is needed. There is no need to have the buck-boost functionality of the LM5118.

    Let me know if you have any questions.

    Thanks,

    Garrett