Hi Guys,
I have a need to do buck regulation, where the regulated voltages are several volts below the positive supply rail. This is a quite atypical setup and it's hard to see any conventional regulators that would handle it.
It seems to me that it should be feasible using TI's digital power chips, so I'm investigating that possibility.
My +ve rail, though, is at around 24V, so chips like the UCD7231 are not suitable. Is that a stopper for me, or are there other ways to handle that? I note in particular that the UCD7231 appears to contain the blanking control for the FETs, which may be an issue.
I'm fortunate that the power is modest at only about 7V and 2A per supply, so I could just ignore blanking and use a schottky diode. Shame though.
Thanks,
Gordon