Hi, team.
Since the maximum rating of EN pin is 3.6 V, when using with VIN = EN, the maximum input voltage is 3.6V?
Can I use it with 3.8Vout/0.8 A at 2.4 to 3.7Vin?
Best Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, team.
Since the maximum rating of EN pin is 3.6 V, when using with VIN = EN, the maximum input voltage is 3.6V?
Can I use it with 3.8Vout/0.8 A at 2.4 to 3.7Vin?
Best Regards,
HI Sir,
Please use a divide resistor to make sure the EN voltage <=3.6V.
Hi, Minqiu
Since it is a battery application, I do not want to waste current to resistance or zener.
Why is EN 3.6Vmax as input voltage range is 4.4V?
Best Regards,
Dear Sir,
you can use 100k and 1M ohm resistor for the divider, thus the current consumption on the resistor is not big.