Part Number: LMR14006
Other Parts Discussed in Thread: LMR14020, TPS560430
Hello team,
my customer has been using the LMR14006 and wants to add another switching to his sensor board. The supply rails are 18V-32V (nominal voltage is 24V); output current is 650 mA @3,3V. The application does directly from 24V to 3.3V and space is critical, so far I've bumped only into devices that require a large inductor.
Do you have any suggestion that requires a small inductor? They are using the lps4018 series of inductors.
Thank you in advance.
Best regards,
Adrian