Other Parts Discussed in Thread: LM317
Hi,
I have a query on the TPS54231,we are using this circuit for a CCTV camera supply.
We are operating with a Li-Ion 14.8V,5.2Ah battery and are charging with Solar Panel.
This Li-Ion battery is acting as input source for the TPS54231.
We have adjusted UVLO voltage at 13.8V for TPS54231 and Output voltage at 11.5V.
The camera at startup spikes to around 300mA to 340mA and settles down to 120mA to 130mA.
The normal operating voltage¤t for CCTV is 11.5V/120to160mA respectively.
During the battery is full condition the CCTV camera is working fine and there is no issue.
But due to cloudy weather conditions sometimes the battery reaches LowerCutoff(LCO)
& during night time and camera gets shut off.
At this point the next day during Day time the Solar panel charges the battery,and it reaches from LCO to UVLO point of TPS54231,
during this transition then the CCTV camera functionality is inconsistent(some times it works and some time it gets hang),
CCTV camera is in Hanging condition means it doesn't work even it gets correct Voltage.
During startup CCTV camera compulsory needs 100mA to 180mA but its not happening.
What could be the reason for this hanging condition ?
Previously we have used LM317 same hanging problem occured there the chance of hanging is 90% but after switching to TPS54231 the chance of hanging went to 50% but we want to completely eliminate thia hanging problem.
As we are installing these Solar based CCTV at customer locations but facing these issues.
Please guide us,quick reply would help us.
Kind Regards,
K.S.S.Phanendra,