Other Parts Discussed in Thread: LP38842-ADJ, LP38842, LP5912, , TPS746, TLV759P, TPS745, TLV755P
Dear Sir/Ms.
What does this form mean?
Is it necessary to maintain Vout on the meter, Vin must be greater than the voltage on the meter?
For example, if Vout=1.5V, Vin must be >2.3V (1.5V+0.8V).
My customer's application is Vin=1.8V, Vout=1.5V, Max Iout=0.5A~1A.
Best Regards,
Kami Huang