I was designing a charge controller for the lead-acid battery using BQ24650. As the ambient (atmospheric) temperature here is around 25 to 30 Deg Celsius we want to use the IC without using the thermistor as mentioned in slva437a.
1) What all changes we need to make to the EVM
2) Is it ok to use without thermistor as the temperature changes slightly around the 25 degrees?
3) Can we give a constant Voltage corresponding to 25 degrees Celsius (from the Thermistor datasheet) across Rp-t?