This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65283: We want the output power to be stable, not to go up and then go down and then go up

Part Number: TPS65283

Dears

Now we have found a problem in TPS65283, there will be a backchannel after the power is started, it is suspected that the soft start time is too short; We want the output power to be stable, not to go up and then go down and then go up. The following is TPS65283 peripheral circuit and oscilloscope display;



The TPS65283, TPS65283-1 output voltage ramps up at the internal slow-start time of 2.4 ms.

 

BRs

Elsa Duan