Other Parts Discussed in Thread: LMR14006, , UCC27282
Hi, Team
My automotive customer is using LM5109B-Q1 in their automotive wireless charger product. They use LMR14006 to convert BATT 12V to 8.3V to VDD pin of LM5109B-Q1.
Customer conduct Power Voltage Drop test on BATT 12V input to system. When the test is conducted, the BATT 12V will drop to 0V with different frequency. The test will last for about 1 minute. Customer require the system should be work correctly after the test, but LM5109B-Q1 can not.
There are HI and LI signal input during the test. After the Power Voltage Drop Test, the LM5109B-Q1 HO and LO output signal duty cycle is smaller than input signal on HI and LI pin respectively. Only power down and power up the LM5109B-Q1 can make it work correctly.
If customer replace LM5109B-Q1 to IR2301, the test is pass.
Is there any suggestion on this issue?
Here is customer shcematic:
Here is hte waveform of BATT 12V.
Here is the waveform on VDD pin during the test. The VDD voltage will drop to as low as 3V.
Thanks
Kevin