Other Parts Discussed in Thread: TPS2378, TPS92513, PMP15004, LMZM23601, TPS92515HV-Q1
Hello everybody,
I have developed a PoE+ constant current source. For the PoE+ PD chip (TPS2378) as well as for the LED driver (TPS92513HV) I chose TI.
With a jumper you can set different currents between 180-700mA.
This works without any problems. The last step was now the EMV pre-compliance, first the wired EN55015... then came the disillusionment.
Exactly at the switching frequency of the LED driver (570kHz) a huge deflection as well as at the next harmonic (1140kHz).
In the appendix you can see the measuring process and the deflections. In the lower frequencies it generally moves very close to the red limit line for the AVG measurement.
Find attached the schematics and PCB Layout for the LED driver. VPOS is 54VDC and at the output there was a LED with 300mA for the test.