On the testing TLC5916, output current is set 15mA by configuration, but test result was 10mA.
Please let me know about why output current was differ.
Test condition is below;
・VDD:5V, 100Ω load
・Control signal(by FPGA) is attached below,
Configuration is 15mA: 0xA6 at special mode and OUT0~5 output: 0x3F at normal mode
・REXT is fixed 500Ω
・Measured OUT0~5 voltage were 1.018V(100Ω load, 10mA)
OUT6~7 are 0V by correct setting
Best regards,
Satoshi