Hello, how do you do ?
This's an engineer from Vtech. We are using your BQ2000SN-B5TR charging IC with 1A charging current to charge a NiMH 7.2V 4000mAh rechargeable battery. To meet the CEC and DoE USA energy saving type approval requirement, we want to disable the top-off trickle charge to save the charging energy.
However, after changed CMTO capacitor value to less than 0.07uF by using 0.047uF for CMTO and 180k for RMTO to set 5.3 hours maximum charging time, trickle charge was still activated frequently when the battery reached full level after fast charging.
Would you please tell us how to change the circuit values to get below result ?
- Battery is connected to the output of charging circuit.
- Provides DC power to charging circuit.
- Charging IC starts charging by fast charge.
- Battery is charged to full level with temperature rise.
- Charging IC detects delta voltage and temperature rise, then stop all charging.
- Charging IC keeps STOP all charging until battery is reconnected or DC power reset.
Thank you!
Best regards,
Fai.