This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62152: TPS62152 output voltage with no input voltage

Part Number: TPS62152
Other Parts Discussed in Thread: TPS62147

Hello, 

I was wondering what happens, when the output sees a voltage with the input floating or grounded? Would that go beyond the abs max of Vin+0.3? So maxmimum would be 0.3 V at the output with no load connected? 

Thanks!

Mat