This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD18535KCS: Switching of MOSFET using optocoupler

Part Number: CSD18535KCS

I'm using an optocoupler for using the CSD18535KCS as a switch. The input pulse to the optocoupler is 3.3V at 50KHz. The output from the optocoupler is a square wave as desired, but after connecting the terminals of the output of optocoupler across the gate and source of the MOSFET, the ouput is not as desired. The charging time seems a lot excessive than desired which I believe is due to the input capacitance Ciss. Any suggestions how to rectify the same?