Other Parts Discussed in Thread: TPS63070
Can you recommend a buck/boost controller similar to the TPS62130A which operates as an LED power supply?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Carl,
Would the TPS63070 suit your design?
Vin=2-16 V,
Vout=2.5-9 V,
Iout=2 A , but this depends on the input/output voltages. In some extreme cases (minimum Vin, Maximum Vout) maximum Iout is below 1 A. Take a look at Figures 13-16, 18, 20, 38, 39, 41 in the datasheet.
Best regards,
Milos