Hi team,
Do we have a device like MAX14913? It is Octal High-Speed, High-Side Switch/Push-Pull Driver.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Eggsy,
The MAX14913 is a push/pull driver capable of driving >0.5 A. The switches and multiplexers are almost all passive devices without drive capability and low power supporting <0.5 A.
What are you using this device for in your system? I may have a low power version of this device TIC12400 depending on what you are trying to do with it.
I typed this device into the competitor cross reference tool and it took me to peripheral drivers so I will move this thread to that forum.
Thank you,
Adam