Previously was pulsing LEDs for 1200us ON-time every 120Hz, with no issue (PWM duty cycle = ~14.4%). Tutring duty cycle up to 95% resulted in either TPS92512HV or catch diode blowing up on board. Output pins of IC now measures a short to ground.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Previously was pulsing LEDs for 1200us ON-time every 120Hz, with no issue (PWM duty cycle = ~14.4%). Tutring duty cycle up to 95% resulted in either TPS92512HV or catch diode blowing up on board. Output pins of IC now measures a short to ground.
Hello Brian,
What is the freewheel diode part number? duty cycle will be high, how long before the buck converter fails after turn-on? If it is long enough for it to heat up can you check the IC temperature? What is your switching frequency?
Best Regards,
Diode Part Number is Diodes, Inc B360A-13-F. Failure occurred almost 1 second after turn-on. LEDs were on, and then about 1 second later there was a snap and they were off. Board will not power anymore. No visible damage to board. All LEDs illuminate using diode setting on multimeter so LEDs are not damaged. Short measured from IC pin 10 (PH) to GND.
Switching Frequency = 700 kHz
Hello,
You have to make sure that is a real measurement. They way to tell is to zoom in and see if it is a triangle/sawtooth waveform. The noise spikes don't count and can be caused by many things such as diode recovery, diode capacitance, MOSFET capacitance, Inductor winding capacitance, noise picked up by the scope probe (check by measuring the GND your probe ground is tied to), etc. Low level signals are sometimes difficult to get accurate so don't always believe what you see on the oscilloscope, verify it.
I forgot to add, when I am troubleshooting a lot of times I'll lower the current set-point way down to prevent damage until I know things are working correct.
Best Regards,
This noise disappears during the PDIM off time
My Vin is stable until the PDIM on time, in which I experience 5-6Vpp of ripple. I have 12 LEDs in a 3x4 grid, so a loop is unavoidable. I am currently on a 2 layer FR4 board, but will be moving to a 4-layer FR4 board.
Hi Irwin,
I was waiting to hear a response from you. The picture I last sent was my ground node measured with respect to another adjacent ground node using a short spring ground. This, to me, shows that I have a tremendous amount of noise in my ground plane when I am pulsing the LEDs.
Do you agree?
Hi Irwin,
I am looking at the EVM schematic. They spec out Vin = 48V, Vout = 5-25V, L = 33uH, and Fsw = 570kHz. These numbers do not jive with the datasheet. The datasheet says to calculate an inductance using the equation 18 with the lowest Vin and the highest Vout and an Iripple of 75mA. Using the Vin and Vout above, and 570kHz and Iripple = 75mA, I calculate a 280uH inductor, while the EVM uses a 33uH inductor. A 33uH inductor in this case should yield a ripple current of 637mA.
This is very confusing. The datasheet says to target Iripple = 75mA, the EVM should have a Iripple of 637mA, and the example application in the datasheet has an Iripple of 89mA (Equation 34)
I am very very confused as to what kind of ripple current I should be targeting in order to size the inductor to my application, because right now I am struggling to fit a 100uH inductor into my design based on Vout = 38.1V and a Fsw of 700kHz. Since I want to run 2A through my LEDs, a 100uH is looking to become very large when saturation ratings come into play.