This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCR022405: soldering bottom layer

Part Number: DCR022405


Hello,

We are thinking to soldering DCR022405P-U and DCP022415DU SOP package to both top and bottom layer of PCB.

Is there any concern or issue to soldering them on top and bottom layer of PCB?

Please let us know if any issue is existing.

Best regards,

Toshihiro Watanabe

  • Hi Watanabe-san,

    From the looks of the SOP package I don't think there would be an issue with solder on top layer of PCB. I am not aware of any issues with the package, however I'd imagine the challenge for this package is when you solder it on the bottom layer of the PCB you might encounter issues with the device during reflow/rework. Unlike the current packages, this package does not have a large EPAD that provides both thermal relief an "anchor" point for the device to sit on. If the device is heavier than the solder tension on the pins then it may fall off during reflow. 

    Regards,
    Jimmy

  • Hello Jimmy-san,

    Thank you for your answer. I think this depends on manufacture company handle or not.

    Is there any other concern you have like performance degradation or shorten life time?

    Best regards,

    Toshihiro Watanabe

  • Hi Watanabe-san,

    Not to my knowledge. I don't think there are any concerns regarding performance degradation of the device if it is used in accordance to the datasheet specifications.

    Regards,
    Jimmy