This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS51604-Q1: mode transition condition (FCC mode <-> very-low-power mode)

Part Number: TPS51604-Q1


Please tell us the mode transition condition. FCCMVLPM. In FCCM, /SKIP = H and PWM = L are set. If /SKIP input voltage is changed from H to 1.6V, will the mode change from FCCM to VLPM? (PWM remains fixed at L.) If /SKIP input voltage is returned from 1.6V to H, will the mode change from VLPM to FCCM? (PWM remains fixed at L.) Or does it need to control PWM?