Other Parts Discussed in Thread: BQ25150
Hello,
BQ25150 has two LDOs :
- an always on Vdd 1.8v LDO <10mA.
- a 150mA LS/LDO which is active by default at 1.8v (e.g. without/before I2C use).
Question 1 : Why setup two LDO's active by default with the same output voltage ?
Question 2 : as 10mA (Vdd max current) is not enough to supply a MCU, what is the exact purpose of Vdd ?
Question 3 : planning to supply a MCU with a voltage other than 1.8v, in my understanding the only way is to add another external LDO wired to PMID. Do you confirm ?
Question 4 : as for BQ2512X, is there any plan to release BQ2515X with different Vldo default values ? (off, 1.8v, 2.5v, 3.3v...)
Thank you