Other Parts Discussed in Thread: TPS7A92, TPS7A84A
Dear TI,
Is there any problem for output capacitance over 200uF.
I intend to use this IC as a cellular module power supply and manufacturer recommended 2mF input capacitance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lucas,
As Clemens Ladisch mentioned both the input and output capacitances are outside of our capacitor limits.
Does your application require the full 3 A rating of the device? If not TPS7A92 which is rated for 2 A may be a better fit for your application as it does not have the same capacitor restrictions. If you do require the 3 A rating, please consider TPS7A84A.
Chapter 2 of our new LDO Basics E-Book discusses the difference between capacitor and capacitance:
Very Respectfully,
Ryan
Ryan Eslinger and Clemens Ladisch thanks for your time.
I am studying other possibilities of a power supply IC, including TPS7A84A.
Regards.