This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61193: TPS61193: Startup flickering of LCD backlight

Part Number: TPS61193

Hi

I am using the TPS61193 to drive the backlight of a LCD display. The backlight is flickering during startup as can be seen on the screenshots of output voltage of the TPS61193 to the LEDs (see image)

Sometimes it takes several seconds to stabilize the LED voltage sometimes it just works without flickering. 

I run with 5V input, 800khz switching, 35mA current limit. The LCD backlight diode string contains a zener diode (rating not specified in datasheet), could this cause some trouble with the TPS61193 ?

Is it normal behaviour that it takes several seconds for the output voltage to ramp up ?