This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24168: BQ24168 Datasheet: Pin 7 is INT or /BATGD?

Part Number: BQ24168


Dear TI

On page 4 of the datasheet of the BQ24168 (the current datasheet on the BQ24168 product page, revision "REVISED DECEMBER 2015") two VQFN 24 packages are shown. The one on the right includes a chip type called "bq241618". I suppose there is an extra "1" there and this should say "bq24168", correct?

If yes, there is a conflict with this drawing (the right package) and the table on page 5. What is pin 7 really? Is it "/BATGD", which is not even described in the table on page 5, or is it "INT", as described in the table?

If pin 7 actually is "/BATGD", can you please provide a helpful functional description of this pin?

Thank you and best regards

Thomas