This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54540: power at output with no input

Part Number: TPS54540

I'm using that part (TPS54540) for 24 to 5V conversion. I'd like to have an additional 5V input connected to its output to be used where 24V is not available.

I'm wondering if that is safe or can be made safe with some modification (like adding an output to input diode as used in linear regulators)