This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A52-Q1: Accuracy deviation over age

Part Number: TPS7A52-Q1

Hello, 

I saw on the datasheet of the TPS7A52-Q1 that the deviation of the accuracy of the output voltage (without bias and between -40°C and +125°C) is -1% and +1%.

I would like to know if it includes ageing.

Thanks, 

Nerea