Part Number: BQ51050B
Other Parts Discussed in Thread: BQ51013B, BQ51003
We have an application where the device might stay on the charger for a prolonged time, let's say several days. The customer wishes that the battery stays close to fully charged while the device rests on the charger.
Now, we are seeing different behaviour on different chargers.
On a Zens PUK2 there is an initial charge after which the charging stops and never restarts.
However, on a Trust Qi charger the behaviour is the desired behaviour; a recharge is triggered whenever the battery voltage drops below a treshold:
Both chargers are WPC compliant and since it is the power receiver that controls the power transmitter I would have expected identical behaviour.
Now, what should I expect? The recharge behaviour of the BQ51050BRHLT we are using in a design is not completely clear to me. In the datasheet of the device, the only mention of recharge is under the 'electrical characteristics' section on page 8; a threshold of -135mV..-90mV is mentioned there. In the rest of the datasheet, appnotes or other documentation there is no mention of recharge.
If we want to accomplish recharge behaviour like in the second image on the Zens charger (which happens to be the approved type), what would be the best method to do so? Would controlling the AD pin from software, tricking the BQ51050B in thinking that there is an AC adapter attached, accomplish this?
Best regards,
Bart van Hest