Hello Team,
The voltage reference of TPS62160-Q1 is given in the datasheet with 800mV typical at TJ 25°C. At room temperature 780mV was measured at the feedback node.
The total given output voltage tolerance is mentioned to be +/-3% over the whole temperature range.
The question is how temperature dependent is the internal voltage reference if there is already a 2.5% deviation at room temperature to achieve the +/- 3% output voltage accuracy?
Best Regards
Joern