Other Parts Discussed in Thread: BQ51013B, BQ500212A
Dear all,
I am using the bq24045 + bq51013B so as to charge a 800mAh battery using also a RX QI antenna (10uH, Imax 3.5A, DCR 0.190 Ohms, Q = 50). When I charge the battery (Iset 550mA) the temperature is ok, around 47 degrees. Once the battery is charged, if I leave my device above the QI TX for hours, even some day, the temperature of the RX antenna remains around 41-42 degrees, but the current is no more than 10-12mA due to a load share circuit which allows to supply my device direclty from the QI system.
I am disconcerted with "high" this temperature because the power in this "standby mode" is much lower than the battery is charging... The I2R losses in the antennas generate heat, but I expected to have a temperature under 40 degrees, and I don't understand it.
My questions are:
1. Is there any equation to calculate the temperature due to I2R losses? Or eficiency vs power losses?
2. How affect the eficiency to the temperature?
3. I want to reduce this temperature and I can't disconnect/disable the QI receiver (I don't have extra GPIO), is there any way for this?
Thank you very much.
Joaquim.