Other Parts Discussed in Thread: BQ25895
Hi.
I am currently using the bq25895 EVM.
I will connect the bq25895 to the solar panel.
If you want to connect the solar panel to VBUS input voltage,
As a result of testing the EVB, we confirmed that when the input power is connected to VBUS, the voltage of the VBUS input power source is output without boosting to 5V at the PMID terminal.
When VBUS input power is removed, it is confirmed that the power of Batterty is boosted to 5V.
Even if power is applied to the VBUS input terminal, if you want to supply the PMID by boosting the battery power,
What should I do?