Dears:
Could you kindly help to check the schematic?
Since there is no output of 5V, and there is no signal testing Nmos' G pot and S pot.
There is no voltage testing FB PIN.
How is the state of PIN31 and PIN32?
Pls. give some advice.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears:
Could you kindly help to check the schematic?
Since there is no output of 5V, and there is no signal testing Nmos' G pot and S pot.
There is no voltage testing FB PIN.
How is the state of PIN31 and PIN32?
Pls. give some advice.
Hi Qian:
Pls. kindly refer the below information:
1. Check if UVLO pin is higher than 1.25V
Luck: Yes, it's higher than 1.25V
2. Check if VCC1 and VCC2 voltage are normal.
Luck: Yes, they are normal.
3. Check if HO1 and HO2 are switching.
Luck: Between HO and Switch's wave as follows:
Btw: the below picture is about between Io and CS1's wave: