This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27200: IR2110 driver circuit works abnormally

Part Number: UCC27200
Other Parts Discussed in Thread: UCC27714, UCC27712

Seniors:
I used the IR2110 driver to build a half-bridge arm drive circuit, as shown below:

The circuit is analogous to the recommended circuit of the manual.

The LIN and HIN pins have a PWM of amplitude 5V and duty cycle of 0.3. The 10V supply of VDD and VCC is stable, but LO and HO do not wave, LO is 0V, HO is 10V. .
Why is this?