Other Parts Discussed in Thread: TPS61020, TPS61099, TPS61022
when i gave input voltage 3.6V then will it give output 3.3V.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Minqiu,
I am giving Input voltage is 3.6V Battery which is variable. when Battery voltage goes to low to ~3V then also output voltage 3.3V should not change.
Hi Zack Liu,
My application requirements
Continuous current : 500mA to 1000mA.
Peak current : ~2A
Input Voltage : 1.8V - 4.2V (Battery)
Output Voltage : 3.3V
Suggest me a regulator.
I am waiting for your reply, my product is on hold , please reply me as soon as possible.
Thanks & Regards,
Bapuji