Hi
I am using the part with the adjustable output. I have 25V in and need 24V out.. But when I power up the output isnt stable. Its moving around a lot. Sometimes I get the same output as the input. Other times its around 24V, about 23.5V but not stable. The sense pin is anywhere between 1.38V and 1.44V. Can anyone see an issues with the attached circuit?
Thanks
Jon